Other Parts Discussed in Thread: TPS2493
Dear colleagues,
I have two questions about TPS2492. I appreciate if anyone has an experience on them.
1. The datasheet of TPS2492 / TPS2493 gives the current sense level in electrical characteristics table as two different levels: 25mV for power limiting enabled (i.e. Vprog < 4V), and 50mV for no-power limiting function active (i.e. Vprog = 4V). However in the rest of the sections including the design application parts and the design tool (slvc033 Excel design calculator) it is only 50mV used.
2. The current sense level, there is a +/-10% margin on current sense reference 50mV or 25mV. I assume this is the production deviation, and is nearly fixed when the part is selected, and the current limit is than dependent only on the temperature effects and the sense resistor tolerances. Could you please confirm this? I appreciate for your helps,
Best regards,
Mehmet DURNA