Other Parts Discussed in Thread: UCC28950, UCC2895
Hello TI.
I am a little bit confused by the way secondary RMS current is calculated in the datasheet. Let me explain what I mean:
According to this:
The picture of the secondary currents will look like:

Where I(Out) is otput DC current (DC component of inductor current). And I(L1) is the inductor current (DCcomponent + AC)
Then there is calculations of RMS currents:

I thought that classical way to calculate RMS value of a DC+Ramp is the follow:
(Numbers are just for example, LTspice shows rms value of a 6.94A for the inductor current)

So can anybody explain what's going on in the datasheet? Why is there Dmax/2 and why instead of just Ims2^2 (DC^2) there is Ips*Ims? And why (Ips-Ims)^2 is not divided by 2? (Ips-Ims=delta I)
Regards,
Vasiliy