This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24707A: Where to connect the ground, it confuses me.

Part Number: BQ24707A


Hello,

It may be a simple and difficult question, but where should I connect the bq24707A IC Grand?

Battery negative terminal according to Simplified Schematic. That is, P_GND?

According to a typical schematic, the adapter and the negative terminal of the battery. In other words, P_GND?

According to the Pin Function, GND is described as being connected to the analog plane. 

I designed the board by connecting it to the signal GND, but the noise synchronized with the switching of the MOSFET overlaps the SMBus.

Is it still the correct way to connect to the signal GND?

Thank you.

Regards,
Shinya T.

  • Hi Shinya,

       Usually these boards are designed to be 4 layer with 2 ground planes, an analog ground and a power ground. The power ground is the reference to PGND and all the high current carrying/switching circuitry ground reference should be connected to PGND. The analog sensitive pins should be connected to AGND so that switching noise does not couple on to the ground reference of the analog sensitive components. The AGND and PGND should be connected with a net tie or 0ohm connection close to IC.

  • Hello Kedar Manishankar,

    Thank you for your reply.
    In this case, I understand that the GND pin should be connected to the Analog ground plane.
    As described in Pin Functions, should the Analog ground plane and Power ground plane be connected only by the via provided under the Power PAD?

    Best Regards,

    Tanaka

  • Hi Tanaka,

       Sure, using a net-tie or 0 ohm resistor near the thermal pad is a valid way of connecting the AGND and PGND. Also the GND pin should connect to power ground.