This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Please introduce LDO.

Other Parts Discussed in Thread: LM7800, LM1084, LM1085, LM1086, TPS7A80, TPS7A92, TPS7A52

Please introduce an LDO with input voltage of 5.5V, output voltage of 5V, output current of about 1.5A to 2A, low noise and fast transient response.

  • Hello,

    LM1084/5/6 and LM7800 would be your best options.

      LM1084 LM1085 LM1086 LM7800
    AEC Q100 NO NO NO NO
    Output Options Adjustable Output, Fixed Output Adjustable Output, Fixed Output Adjustable Output, Fixed Output Fixed Output
    Iout (Max) (A) 5.5 3 1.5 1.5
    Vin (Max) (V) 29 29 29 30
    Vin (Min) (V) 2.6 2.6 2.6 7.5
    Vout (Max) (V) 27.5 27.5 27.5 15
    Vout (Min) (V) 1.25 1.25 1.25 5
    Fixed Output Options (V) 3.3, 5 3.3, 5, 12 1.8, 2.5, 3.3, 5 5, 12, 15
    Enable NO NO NO NO
    Power Good NO NO NO NO
    Output Capacitor Type Non-Ceramic Non-Ceramic Non-Ceramic Ceramic, Non-Ceramic
    PSRR @ 100KHz (dB) 30 30 30 48
    Noise (uVrms) 38 38 38 40
    Accuracy (%) 1.5 4 2 3
    Vdo (Typ) (mV) 1300 1300 1300 2000
    Iq (Typ) (mA) 5 5 2 6
    Thermal Resistance θJA (°C/W) 23 23 23 24
    Min Package Area (mm2) 46.5328 46.5328 16 45.5
    Package Type DDPAK/TO-263, TO-220 DDPAK/TO-263, TO-220 DDPAK/TO-263, TO-220, WSON DDPAK/TO-263, SOT-223, TO-220

    Regards,

    Prakash L

  • Thanks for the introduction.
    Is there anything similar in the latest small size like the TPS series?

  • We only have Adjustable Vout options in TPS series like TPS7A52, TPS7A92, TPS7A83 that can meet your 1.5/2A requirements. If you need fixed, the closest is TPS7A80 which has a max Iout of 1A.

    Regards,

    Prakash L