Hi,
I'm currently designing a circuit to charge a battery pack using the bq2000t. As of now this circuit was designed to charge three NiMH AA batteries in series but for my purposes I was wondering if it was possible to increase the capacity of my battery pack. My thinking was that if I put three more batteries in parallel with the original three NiMH batteries i could double the battery capacity. By doing this however, I was wondering if I'd run into a few problems. For instance: would the current output of the bq2000t need to double or would having these extra batteries also raise the rate of heat measured by the thermistor? I guess my main question is what would I have to change in my battery charging circuit that would allow me to put another three NiMH batteries in parallel to the original three. Thanks in advance.