Other Parts Discussed in Thread: TL432, TL432LI, , ATL431LI
Hi,
Because the TL432 and TL432LI are out of stock, and ATL432LI we has stock,
so I want to use ATL432LI to replace the LA431OCRPA, and the datasheet as the following link, but the customer consider that the Ika is too low (15mA max),
http://www.liteon-semi.com/upfiles/tecfile01445239981.pdf
And you can see the schematic with the calculate was 19mA ((Vo-0.7)/R306=(30-0.7)/1.5K=19.53 mA). Is that ok for used the ATL432LI?
Or are there other calculation methods that can convince the customer? thanks.

Best regards
Rock