This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS82130: EN pin defect

Part Number: TPS82130

Dear TI Team,

we had some defects on the EN pin of the TPS82130 device. We reckon it comes from the VIN+0,3V abs-max-rating in the datasheet. We do not fulfil this rating, because there is a 100nF capacitor next to the pin.

Is there a protection diode on the EN pin existing?

BR,

Wolfgang

  • Hi Wolfgang, 

    It is not recommended to operate above the recommended operating conditions. Exposure to absolute-maximum-rated conditions for extended periods may affect device reliability. the device is not protect above the abs max. 

    thanks! 

    Tahar