This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100: Creating Golden Image Reset Estimated Capacity

Part Number: BQ34Z100
Other Parts Discussed in Thread: BQSTUDIO,

I was using Battery Management Studio to create golden images for a Fuel Gauge that was calibrated and showing a good estimated capacity. Immediately after the golden image was created the estimated capacity went from 40% to 0%. 

Why is that? Looks like I will need to cycle the battery again, which is frustrating, but also does this mean the golden image will not be valid and I will need to do learning cycles on batteries that are loaded with those golden images? Learning cycles are incredibly time consuming in production for an 8S battery.

Also in production I am using the .df.fs golden image. I'm unclear if that contains all the information from the learning cycle. I know it covers the other calibration data.

I've been having an issue where the 8S battery is showing 0% at 27V and I've been trying to get them to show 0% at 24V. 

I'm using bqstudio 1.3.101