This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25700A: Replace a BQ25703 with a BQ25700

Part Number: BQ25700A
Other Parts Discussed in Thread: BQ25703A, TPS65987D

Hello,

I would like to replace the BQ25703A with the BQ25700A following the schematic below, They're pin to pin compatible and the datasheet are very similar, they only difference is that the BQ25700A communicate (host control interface) with the USB/PD Controller thourgh SMBus when the BQ25703A communicate with the I2C Bus. The I2C and SMBus are very similar, on the datasheet they have the same power rail and the same pullup resistor value.

So, is it possible to make a schematic of power delivery with TPS65987D and BQ25700A ? (Max power charge <45W)

  • Hi Alan,

    They are pin to pin compatible parts. Please see difference below.



    I am not familiar with TPS65987D (for example, whether or not it can do SMBus), so I would recommend posting a new thread with TPS65987D as the title. In terms of power capability, you can replace BQ25703A with the BQ25700A. In other words, if TPS65987D is capable of SMBus and capable of the same communication commands, then it should be ok.

    Thanks and I hope this helps,

    Peng

    *Please press "This Resolved My Issue" on the thread if my answer is satisfactory