Other Parts Discussed in Thread: LM3409, TPS92515
Hello,
I have an application whereby we need to drive a high brightness red LED (Vf = 2.1V) at up to 1A. Input voltage was planned to be 24V but we also have 12V rail and 48V rail available if that is better.
We need the analog dimming because a photo diode is measuring reflected light from the sample that the LED is illuminating. Low flicker is needed.
Will the TPS92518 work for this application? If not do you have a part that you would recommend instead?
Thanks,
Derek
P.S. part needs to be in stock somewhere in the world so we can buy it.