This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62866: VIN related questions

Part Number: TPS62866

Hello,

My customer has some questions about TPS62866.

Q1:

Looking at Figure 8-1 of the datasheet, VIN rises first then EN ramps.
But, VIN and EN can be connected and they can ramp simultaneously?

Q2:
They would like to confirm tF_VIN spec.
VIN falling slew rate has to be farter than 10mV/us?
Or VIN falling slew rate has to be slower than 10mV/us?

Q3:
If tF_VIN spec is violated, what would go wrong specifically?
Could you elaborate, please?

Best regards,

K.Hirano