Other Parts Discussed in Thread: UCC256402, UCC28180
Hi there,
I managed to design a power supply that meets my PVDD requirements (for driving multiple Class-D amplifiers) using WEBENCH, but I'd like to include a second Vdc output to drive the logic on my PCB's too. Is it possible to setup WEBENCH to design a power supply with dual (or even 3) different output supplies?
My design requirements:
240 Vac (10 A 50 Hz supply here in Australia) as input voltage source
Output 1: 24 Vdc, max 30 A (isolated so no/very low switching noise in the outputs)
Output 2: 5.0 Vdc, max 3 A (again isolated)
Are you able to assist me with this please?
Many thanks.
Mark