Using Version 7.6.1.
This version of Fusion Digital Power Designer requires many more clicks (and much more steps in my test procedure) to change one of the power rails on a Xilinx FPGA board, than it used to take with the old version. I don't know if it has to be that way - am I missing some way to dock some windows? Trying to keep the procedure simple for some technicians, etc. Procedure was all complete and now a new test computer with new version of Fusion Digital Power Designer is going to require many more steps.
This used to be very simple. I am just changing one power rail from 2.5V to 3.3V on a KC705 xilinx FPGA development board that has three UCD9248's.
Here's what I want to see, (screen shot of old version of Fusion Digital Power Designer (2.0.89) from our test procedure), and everything was done on one screen:
Here's what I see now: I have to click "configure device" to open a separate window, then select the correct rail in a drop-down at the top. Am I missing something? Did the software get much more difficult to use or am I missing some mode or window to enable editing all in one window? I am hoping I am just missing something so I don't have to screen-shot windows, etc to rewrite the procedure.