This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3808: How to set adjustable reset time to 10 second

Part Number: TPS3808


In the datasheet of the material, the adjustable reset time is shown as a maximum of 10 seconds.but it is necessary to use a capacity of approximately 1.74 uf to set 10 seconds ( 8.3.2 equation 1) .It is difficult to find a capacity of this value in the market.

Therefore, to capture this value, for example, use 2 capacite  -> 1.5 uF and 0.22 uF. ( sum of 1,74uf) Is this a viable method?

Or if we put a 2.2uf capacitance(greater than the calculated value) on the ct pin instead, can we provide a 10 second delay? Does it cause problems?

which way should i use?

Best regards.