Hi,
Could you please suggest me a 50A regulator?
1. Input voltage - 5V.
2. Output Voltage - 0.72V
3. Output Current - 50A.
4. Soft start - Better if its around 0.5ms.
5. Type - Good if its step down converter
Earlier we were using two 40A regulator TPS543C20 .Now since the current requirement is reduced we planned to switch to one 50A part instead.
Thanks & Regards,
Nireeksha