We have need of a switcher that can maintain a voltage of 3.3V when the supply is 2.7V and 3.6V. It also needs to supply 2A peaks to a 3G Cell phone module as well as powering an ARM processor.
Since all the devices on the 3.3V rail can handle 3.6V, there is no need to use a more complicated solution (eg TPS63020) which is hard to source at present due to lead times.
My question is.. what will the device do when the voltage climbs to 3.3V and above.
Thanks
Simon