This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25600: BQ25600

Part Number: BQ25600

Hello. I have some questions of bq25600

1) Do I understand correctly that the VBUS pin can work as both a charging input and a boost OTG output?

2) If The PMID pin its out of boost converter and i use that for supply? What a max current drive this pin? 1.2A? And what in this pin when i plug adapter to VBUS pin?

3)What a maximum current of VSYS  i can use?