This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM5601R5H: PGOOD Maximum current

Part Number: TPSM5601R5H


I would like to drive a status LED with 5 mA to indicate the PGOOD status. The datasheet does not list a maximum current specification for the PGOOD pin. Could it support the 5mA LED drive current?

  • Hello Jamie, We havent characterized the sink capability of PGOOd on this particular device. Typically, it is driving a high-z impedance in practice. Looking at other devices, I see absmax of sink current being 5-10mA. You might want to consider only using PGOOD to drive BiPolor or MOS gate and keep to a couple mA max.