Hello
I am wondering that if , from your experience, is it common to use in a product both rechargeable and non rechargeable batteries (1 or 2 in paralell , CR123) and the product to have embbeded a charger for when the user puts rechargeable battery. It has also a buck-boost converter whoch regulates to 3.0V in order to accomodate the 2.0 - 4.2 V range (2.0-3.2 non rechargeable, 3.0 - 4.2 V rechargeable)
I need to discriminate which kind of battery did the user put, or at least to protect the system if he tries to charge a non rechargeable battery.
My brief research on this matter did not revealed to much informations.
Any ideas and thoughts regarding this tipic? How does a nonrechargeable behaves when you try to recharge it? How should I protect the system.
Thanks