Hi all
My customer has a design using the LMR14010A, the specification is:
5V .... 32V => 3.3V/50mA, the device is mostly running in eco-mode.
They see a ripple of 40mV ... 60mV, which is too high for their application and is affecting the ADC accuracy.
What measures can you recommend to reduce the ripple in eco-mode ?
.... or is there another comparable device at comparable cost that you would recommend using ?
Please find the schematic copied below.
Best regards
Ueli
---------------------------------------