This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AC-DC conversion

Hi,

I want to design a Ac-Dc PFC  converter.  For 230v rms input how to select Vin min and Vin maximum. In general foe any given circuit how to select Vin min  and Vin maximum value??

  • Hi Mownika, 

    VIN min and max are the RMS line voltages you expect to see in your application plus a buffer to accommodate variance.  For instance, 85-265V is considered the "universal" line range which covers 100Vac (Japan) to 230Vac (Australia/India) with +/-15% limit variance.  If you're designing for a single source only, such as 230Vac, you may use 195Vac - 265Vac (+/-15%) or modify the buffer to accommodate a wider potential variance.  Generally, you want your circuit to operate across the expected line variation yet take appropriate measures to an under/over-voltage condition.