This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25723EVM: Start charging of cells without programming

Part Number: BQ25723EVM
Other Parts Discussed in Thread: BQ25723, EV2400

Hi,

I'm trying to evaluate the BQ25723 by charging two 18650 cells with the Evaluation board (BQ25723EVM). If I understand the datasheet correctly the default charging voltage for 2S should be 8.4V. It also states that the charging will start when the host writes the charging current. At the moment I don't have a EV2400 Communication Kit available. Is there a way of starting the charging without connecting the I2C header?

Best regards,

Simon