Other Parts Discussed in Thread: UCC28070, , UCC28950, UCC28070A
Hi support team,
I am looking for a 2-output ACDC converter with the following specifications.
Can this be achieved with this IC?
Please let me know if there is another suitable IC.
ACDC converter specifications
・AC Input Voltage Range: 85 to 264V
・DC Output 1: 60V, 10A
・DC Output 2: 12V, 30A
・Isolated : Yes
・Application: Large capacity charger
Regards,
Dice-K