Other Parts Discussed in Thread: BQ24773, BQ24780
Hi,
We are using BQ24780S charging circuit in our unit, it has to work with both 12V and 24V Battery.
we have 10mtr cable between the Battery and the unit, so the ACDET Divider circuit i used was 470K and 178K in order to work from 9.8V to 24V as ACDET absolute max is 6.5-7V.
Now the problem is the charger has to work at 9.8V, but it will work properly only at 10.7V with the load of 1-1.5A for 3S during TX, else around 0.6A regular,. and with cable of 10mtrs, it is working only after 12.7V, else charger is resetting means the charger goes off when tx happens with high current hence failing.
Charger parameters like Charger i/p current, Discharge current windows are in max,.
one experiment i did by changing ACDET to 470K and 324K, R1/R2 then it works fine from 11V itself with 10mtr cable, but problem is it is nt safer range at 24V input for the charger, as ACDET goes beyond 7V.
what if i increase ACDET above 7V ? will it effect the charger? any other means to verify that the charger with load and cable length nt effecting charger performance at lower vtg inputs.
help me out to solve the issue.