This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92200: Ripple current typo

Part Number: TPS92200

HI,

The TPS92200 datasheet on page 18, states:

"For TPS92200, TI suggests that the inductor current ripple be larger than 300 mA to assure loop stability. If the
calculated inductor current ripple is less than 300 mA, TI suggests a smaller inductor."

But all the examples use a ripple current of 30mA or less.

Was it a typo and does the ripple current need to be larger than 300 uA?

thanks for your time Nadir