This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65920 duty cycle problem on 32k clock

Hi,

On my OMAP board, the 32,768 Hz clock is a square clock provided by an external RTC.

The duty cycle of the clock is at about 40%, and I just noticed there is a requirement of 45/55% in the SWCS037E datasheet.

The OMAP on its side does not require a particular duty cycle on this clock.

 

What could be the consequences of this duty cycle issue on the PMIC ? I won't be using the PMIC's real time clock, but I think that the 32k is used widely in the PMIC for other functions.

Regards

Philippe