Other Parts Discussed in Thread: TPS2493, , GPCCHEM
Hello,
We use the BQ34Z100-G1 together with a TPS2493 due to a requirement. This enables us to switch off the voltage in the event of a short circuit.
This circuit has a power consumption of approx. 1mA, the supply of the component is in front of the shunt of the BQ34Z100-G1. We have seen that this causes a significant error in self-discharge estimation.
Is there a way to adjust this value so that we get better results there?
Would it make sense to put the supply of the TPS2493 behind the shunt - I don't think so, because we have configured 40mA quiescent current, or is it still recorded internally and used for the self-discharge estimation?
If further information is required, I can add it if necessary.
Regards
Mathias