Hi,
I'm designing a buck-boost converter and in the datasheet (https://www.ti.com/lit/ds/symlink/tps55165-q1.pdf?HQS=dis-mous-null-mousermode-dsf-pf-null-wwe&DCM=yes&ref_url=https%3A%2F%2Fwww.mouser.es%2F&distId=26) I have seen that a maximum DCR is stated for the inductor in section 7.5. A maximum of 40mOhm is stated as the requirement.
The inductor I'm planning on using has a higher DCR of 120mOhm. However the load has a fairly high resistance, around 60Ohm, resulting in a ratio between Rl and DCR of 500. The output voltage is 12V, in case that matters.
Could you provide any information on why is there a DCR requirement in the datasheet? What are the expected consequences to not following this requirement?
Thanks and regards.
Nicolás.