We're running a BQ34 on a number of 54Ah 12V lead-acid battery packs. We've run into an issue that when we reduce the load on the batteries from the active load of between 1.0 and 2.4A to a standby load of 50 mA, the capacity indicated by the batteries will almost immediately drop from well over 50% remaining to 12% or less remaining, and it will then often drop to 0% remaining. The pack voltage and other tests have shown that there is still the previous >50% capacity still in the batteries. Any idea what could be causing this?
Thanks,
Peter