The kit provides up to 5v @ 1A, are there design notes for increasing the power and/or the voltage by a factor of 2 or 4?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The kit provides up to 5v @ 1A, are there design notes for increasing the power and/or the voltage by a factor of 2 or 4?
The present low power WPC stanadard is 0 to 5W (5V at 1A). We are supporting the low power standard at this time, but not higher power applications.
If you only require additional voltage it may be possible to covert the 5V to a higher voltage through a boost converter, TI has a large number of them.
Thanks for the clarity on the TI Ref design wrt WPC standard. I've got a prototype that uses a different processor as PWM source and control of resonant frequency for regulation and was hoping to switch to the TI controller. I'll do some more study of the controller and it's adaptability to my design requirements.
Thom,
If you like to further discuss applicability of BQ500110 to your design you may contact me directly at Vladimir_muratov@ti.com.
Best regards,
Vladimir Muratov
Texas Instruments
DC Solutions
Wireless Power, Tx