Hi TI support,
I have designed a 4-layer PCB with the same design parameters as the LM5175 datasheet:
Vin =6-36V,
Vout=12V,
Iout=6A,
Fsw=300kHz
And was hoping that someone here could take the time to review it.
I intend to use the same layout for another board that will output 24V, 3.5A.
Best Regards,
Ritchie