Other Parts Discussed in Thread: TPS731,
Hello guys,
One of my customers was going to use TPS73115 for their new product mass-productions.
But they knew it was difficult to prepare the device by their due date because TPS73115 lead time is too long.
So they decided to use TPS73615 instead of TPS73115 because the device lead time is very short.
At this moment, they have several questions as the follows.
They want to understand that TPS73615 is almost same device as TPS73115
because they want to know it is no problem to replace TPS73115 to TPS73615 through your replies.
Could you please give me your reply for them?
Q1. Is the different point between TPS73615 and TPS73115 the current limit circuit only ?
Q2. Are other circuits same between these devices?
Q3. In the device final test, is the current limit function tested with each device spec value?
Q4. When TPS73615 is used around 100mA on the lower limit side, are the device characteristics same as TPS73115?
Your reply would be much appreciated.
Best regards,
Kazuya.