Other Parts Discussed in Thread: LMZ31704, LMZ31710, , LMZ31707
Hi,
We would like to replace our existing designs having LMZ31710,LMZ31704,LMZ31707 DC-DC Switching Regulators with TPSM8A29 due to non-availability of stock.
1. Using the current limit pin(TRIP) on the TPSM8A29, can we configure this to customized current rating. Doing so will this be stable?
2. In the TPSM8A29 there is provision for multiple switching frequencies, what are the advantages of having these frequencies? How to chose the correct mode and suitable frequency?
3. Instead of using 8 output capacitors shown in application schematic, can we use only 4 capacitors? if so do we need increase the output capacitance?