Other Parts Discussed in Thread: BQSTUDIO, , BQ34Z100
Hello
I am having a problem with writing parameters in BQStudio. How can I write to BQ34Z100-G1 ?
For example, when I try to write the value of OT Chg from 45 to 55 in the Data Memory window, BQStudio said "A read of data written failed comparison" and the value remains at 45. Also, even though I press "Write All" button after pressing the "Imports Defaults button", It said "Parameter not written. Class name Gas Gauging, Subclass name State,...". and the parameters will be left as they were.
The following is what I tried.
・I2C communication with BQStudio is possible.
・I Could write to the same board before. This problem occurred when I tried again after some time.
・The same problem occurred with another board.
・Commands such as SEALED and UNSEALE can be sent.
I will also attach the data.211012_DataMemory.csv
Tue Oct 12 09:46:54 JST 2021 Device Version Info = 0100_0_16 BQZ Device Name = bq34z100G1 BQZ Firmware Version = 0_16 Sample,DateTime,ElapsedTime,Control,CtrlStatus,StateofCharge,MaxError,RemCap,FullChgCap,Voltage,Current,AvgCurrent,Temperature,AverageTimeToEmpty,AverageTimeToFull,AvailableEnergy,AveragePower,InternalTemperature,CycleCnt,StateofHealth,ChargeVoltage,ChargeCurrent,PackConfig,Flags,Flags B,GridNumber,LearnedStatus,DoDatEOC,Qstart,TrueRC,TrueFCC,StateTime,DOD0PassedQ,DOD0Time,DOD0,QmaxDOD0,QmaxPassedQ,QmaxTime,LogRowTime(ms),LogStatus 1,2021-10-12 09:46:59,5.152,0x0016,0x0215,0,100,0,3916,4636,0,0,14.9,65535,65535,0,0,24.0,0,88,8200,5000,0x2F61,0x0116,0x2400,15,4,3392,3916,-33,3916,436,31,3,16228,0,31,3,919,SUCCESS