We bought the above regulators from mouser (Purchase order no. TIFR/1180317/12P0213) in Feb 2019.
We observed that the output of the regulator while using ANY-OUT programmable operation varies from IC to IC and thus the programmable combinations
had to be changed from module to module in our design. Below are the measured voltages at different pins of three ICs
IC1 IC2 IC3
Pin 3 (Fb) 1.037V 0.884V 0.970V
Pin 13 (NS/SS) 0.778V 0.778V 0.778V
Pin 1 (Vout) 1.037V 0.884V 0.970V
when programmble pins are open
We didn't face the above problem in the regulators that we got as samples (TPS7A8300RGR)