Hi,
Currently, the semi-automatic mode we use is configured through the I2C bus, but the TPS23861 will always send out detection, resulting in a 19V voltage pulse on the network port.
(Any other solution to prevent the voltage pulse?)
I would like to ask, in the semi-automatic mode, can the detection negotiation be realized through interruption?
That is, after inserting the PD device, the detection is performed by interrupt mode.
When the PD device is not inserted, or other non-POE network port devices, the detection action will not be performed.
if nor, any other software solution?