Other Parts Discussed in Thread: TPS630242, TPS63030
Hi,
I was looking at the TPS63000 datasheet and noticed the split VIN and VINA pins, and wondered if VIN and VINA could have different voltage supplies, i.e. VINA > VIN.
I have seen a previously resolved post on this forum regarding the TPS630242, however the question asked there was what happens when VINA < VIN.
Some background. I am looking to connect VIN to a solar panel, and use the TPS63000 to charge a battery. The idea was that perhaps, if the control stage (VINA) can be supplied by the 2.5V+ battery, the power stage (VIN) might continue regulation below the recommended minimum 1.8V input voltage, and the battery would continue charging at lower solar panel input voltages.
Thanks in advance.