Hi team,
I got a question from customer.
"
In the Application Report Loop Response Considerations in Peak Current Mode Buck Converter Design SLVAE09B – JULY 2018 – REVISED AUGUST 2021 and in other publicly available established engineering texts the following is needed to do a full analysis:
1 - Ri; the current sensing resistor or its equivalent value
2 - The transfer function of the error amplifier
3 - The compensation current ramp slope (change in current over time)
Also, in the modulator section of a controller there is at the input to the PWM comparator the valley and the peak of the ramp. The values of this are necessary to properly simulate the circuit. In the UCx84x variants Current-Mode PWM Controllers datasheet (www.ti.com/.../uc2845.pdf in Figure 11 and Figure 12 the almost universal circuit between the E/A and the PWM comparator is used. I suspect the same exist in this part. Can I use the same values for the valley and peak as is used in this diagram? I have figured out the resistor values and diode drops for this circuit by analysis.
Please provide this information. It should be in the datasheet.
"
Thank you very much for your help.
Best regards,