Other Parts Discussed in Thread: LM25145
Good morning,
What would be the short circuit behavior of this IC?
Thanks a lot for your help.
Best Regards,
Onur
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Onur,
This device does not have short circuit protection and will be damaged from a short circuit fault if no external short circuit protection is used. If you're looking for a device with the short circuit protection feature you can navigate to the load switch portfolio and sort by features.
Regards,
Kalin Burnside
Hi Kalin,
Thanks for the quick feedback. I have a 5V Switching supply on my circuitry with a short circuit protection kicks in when the load is above 6.8A. The output of this switching supply is connected to TPS22990 which is capable of delivering 10A.
When I short the output of TPS22990 and power the circuit up, I don't see any current driven from 5V switching supply and I see the output of the switching supply as 5V. This made me think, if there is a short protection circuit in the TPS22990.
Maybe I shouldn't just start Load switch output as shorted but I short it during operation to see if short circuit protection of the switching supply kicks in.
Hello Onur,
Can you please provide a waveform including Vin, Vout, Iout, and EN of the TPS22990?
If the device is enabled and this event happens the input voltage should drop. The only way I can see this event occurring is if the TPS22990 device is disabled.
Regards,
Kalin Burnside
Hi Kalin,
On monday I will go to the lab again.
1-) I will connect an external load to the output of TPS22990 and start increasing the load to see the behavior of my circuitry.
2-) I will short the output of the TPS22990 when the board is on and check if LM25145RGYR current limiter kicks in.
3-) I will short the output of the TPS22990 and check the behavior again.(this was my initial test)
I will share the results with you hopefully on monday.
Thanks a lot for the help
Best regards
Onur
Hello Onur,
As I haven't heard from you in 18 days I assume you've figured out your issue. I will now close this thread.
Regards,
Kalin Burnside
Good morning, I did some tests and current limiter of LM25145 kicks in so I don't see an issue.
Best Regards
Onur