Hello team,
In my application I don’t need the 3rd string of the LM36923H.
Can you help with the questions below?
- I do not intend to use the PWM input, only the I2C. Therefore, the question is do I leave pin unconnected or should pull high or low?
- When using the LM36923H, the 3rd string input LED3, which will not be used, do we leave just unconnected or should it be pulled high or low?
Thanks!
Connor