This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78350-R1: max error update

Part Number: BQ78350-R1

 BQ78350-R1 MAX ERROR is not update to 2, Which parameters affect?

  • Hi, 

    The Max Error should update when the device has had a qualified discharge to the EDV2 voltage which will cause it to update the learned Full Charge Capacity. If the Full Charge Capacity is never updated, the accuracy of the gauging will decrease over time as the battery ages.

    Best regards,

    Matt