Part Number: TPS3430EVM
Other Parts Discussed in Thread: TPS3430, TPS3850
Hello everyone,
I was trying to design watchdog timer circuit with latched output, means that WDO will give constant LOW (0V) when watchdog pulse is missed or not in the watchdog window, otherwise HIGH (5V or 3.3V).Luckily I found TPS3430 Watchdog IC , when I check the datasheet, in page 24 section 8.2.3 they have example circuit for latching window watchdog timer.I tested the circuit and it works as expected, although I had to add manual reset, but it worked fine.
Unfortunately, currently it's not in stock.
So my question is; Is there any other IC by TI that provides similar functionality and latching capability of TPS3430 watchdog timer IC.
Thanks in advance for all replies and suggestions.