We're hoping to use a TPS5450 at 4A-5A (continuous) to supply power to various loads consisting primarily of small incandescent bulbs, switching battery chargers, and LED drivers (for task lighting).
The cable length from the TPS5450 to the load can be as long asy 4 feet (8ft. round trip). Are there any changes you'd recommend making to our SwitcherPro-generated designs to make sure the output remains stable? If necessary, I'll trade some transient response for stability as most of the loads don't change after the load is connected, or the load changes slowly. Unless the input ripple to something like a DC-DC battery charger located 4ft away requires good transient response.