We're hoping to use a bq24707-based charger in our next design and I was wondering if there were any changes recommended for handling long output cables? Assuming that our circuit is similar to the one used for the EVM and that the cable to the battery can be up to 4ft long (8ft. "round trip"), is there anything we should be worried about? Typical charge current levels are 2A and 5A at 14.0V - 17.0V.