Part Number: BQ25672
Other Parts Discussed in Thread: , USB2ANY, EV2400, BQSTUDIO
I have a BQ25672EVM connected to one PSU on VIN1, nothing on VIN2 et USB connector, one 5W 100ohm resistor between SYS pin and GND, one cell LiFePO4 battery on Battery port.
I checked VAC1 is 5V.
I have no connection to PC to configure chip.
VBUS is floating except if I bypass VAC1 to VBUS with JP3.
Why?
Same thing if my PSU is connected to VIN2.
Does BQ25672 need anything else to activate ACDRVx when
I have a BQ25672EVM connected to one PSU on VIN1, nothing on VIN2 et USB connector, one 5W 100phm resistor between SYS pin and GND, one cell LiFePO4 battery on Battery port.
JP30 and JP33 are shunted to provide 3.3V to USBANT. I checked PULLUP is at 3.3V.
I have one USBANY card connected to my PC.
I first downloaded Browser extension, then TI Cloud Vinx is the only available power source?