Hi everyone,
I am currently designing a Li-Ion battery charger to power a Raspberry Pi 4. I will be needing to use a 3.7 V 4500mAh ~ 5000mAh battery. I am not very familiar with power electronics and battery management, however, after some research I know I am in need of a battery charger IC (switching charger, since the high current), a battery fuel gauge, and a boost converter to deliver 5V and 3A to power the RPI4.
I am not sure what I need to take into account when selecting charger, fuel gauge, and boost converter. So knowing the battery that I need to use, does anyone have suggestions about which components I could use? I was looking into the BQ24170, but I am very unsure.