This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25300EVM: BQ25300EVM

Part Number: BQ25300EVM
Other Parts Discussed in Thread: BQ25300

I want to use a 12V 1A input supply instead of 5V 3A to this board. "Power Supply #1 (PS1): A power supply capable of supplying 5 V at 3 A is required. While this part can
handle larger voltage and current, it is not necessary for this procedure". The BQ25300 circuit can handle 17V according to data sheet.

Main test case will be a 2A output to a LiFEPO4 battery.

Question? What do I have to change, if anything, to handle this input voltage of 12V?

BR   Bengt S.