This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610: What is the correct connection of D1 cathode?

Part Number: BQ24610

The BQ24610 EVM has the D1 cathode connected between R14/C16 whereas the data-sheet has the D1 cathode connected directly to BTST. Which one is correct? I always lean towards the EVM design as it obviously works, but this seems to be the exception in this case and the data-sheet and design checklist have the D1 cathode connecting directly to BTST.

  • R14 can be used to slow down the BTST charging pulse which helps with EMI. Even if not requiring, BTST R, it is still good to include a 0 ohm R if it is required later on in prototype testing. You are right that EVM should be followed closer. The datasheet will show typical operation.