This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5145-Q1: Design components specifications

Part Number: LM5145-Q1
Other Parts Discussed in Thread: CSD19533Q5A

In a project, I want to integrate LM5145-Q1 with the following specifications:

Vin:  24V to 75V (44-50V typical)

Vout : 12V

Iout max : 6A

According to excel calculator (in attachment) and Webench, M1 is CSD19533Q5A and M2 is FDMS86101.

Can you check that choice is a good one ?

Thank you for your help.

LM(2)5145, LM5146 contorller design tool - revA1.xlsm