Hi Team,
Can you estimate the approximate conversion efficiency curve (Pi/Po) in Input voltage 8~16V and LED condition as below:
- LED constant current 1.2A ± 0.1 A
(1)LED Voltage is 12V
(2)LED Voltage is 8V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Can you estimate the approximate conversion efficiency curve (Pi/Po) in Input voltage 8~16V and LED condition as below:
(1)LED Voltage is 12V
(2)LED Voltage is 8V
Kevin,
I suggest that you obtain EVM and do the measurement since this can vary quite a bit depending on load an input voltage variation. In general in can vary from 70% efficiency to 85%.
Thanks Tuan